World record
The full project comprises of a ± 320 kV extruded HVDC underground cable turnkey system. This includes the engineering, production and installation of two 600 MW bipolar circuits along a 190 km land route between the substations of Piossasco, near Turin (Italy) and Grand’Ile in Savoy (France). The cable will cross approximately 95 kilometres in each country. The link is the longest of its type and sets a world record for HVDC underground interconnections using extruded cable technology.
“Prysmian Group will be coordinating the design, supply, installation - including civil works - and commissioning of the interconnection,” explains Alessandro Panico, Sales Manager. “Together with Silec Cable, we will provide the HVDC underground cable systems. These are insulated with extruded material technology. Roda S.p.A. and CEBAT srl will provide civil works and installation on the Italian side and Gauthey, Serpollet and Sobeca will provide civil works and installation on the French side. This project re-affirms our worldwide leadership in the strategic high valueadded sector of HVDC grid connection projects.”
Track record
“The client needed a secure power supply and power exchange between Italy and France. To realize this, we had to take into account an extremely complicated installation route with tunnels and viaducts. Prysmian has an undisputedly wide track record in HVDC cable – possibly the largest amongst competitors - and we also underwent a long qualification programme”.
Prysmian Group recently announced the successful commissioning and hand-over of the HVDC offshore grid connections BorWin2 and HelWin1 and the DC land section of Skagerrak 4. Two further DC offshore grid connection projects, SylWin1 and HelWin2 are nearing completion. Prysmian is currently also involved in the HVDC cable systems for the DolWin3 and BorWin3 projects. Another HVDC interconnection (France - Spain) realized by Prysmian is near completion and will start operations shortly.
“We are proud to make our technologies and our experience available to the realisation of a project with such a high strategic value” said Valerio Battista, Prysmian Group CEO. “The development of power transmission interconnections is of paramount importance in Europe and Prysmian is a key player.”